Încercaţi să căutaţi în funcţie de cuvinte-cheie, codul produsului sau codul de comandă ori numărul de serie, de exemplu, „CM442” sau „Informaţii tehnice”
Introduceţi cel puţin 2 caractere pentru a începe căutarea.
Understanding how the different ultrasonic sensors work
ArticleMai multe industrii03.12.2024
Pe scurt
Ultrasonic flow measurement uses ultrasound to measure flow rates through three methods: transit time differential, Doppler shift, and cross-correlation. The transit time method is the most accurate and widely used, applicable to liquids, gases, cryogenic, and high-temperature applications.
Ultrasonic sensors come in three types: clamp-on, insertion, and inline. Clamp-on sensors measure flow from outside the pipe, insertion sensors are in direct contact with the fluid, and inline sensors are pre-installed in measuring tubes for high accuracy.
CuprinsCuprins
Ultrasonic flow measurement
The field of ultrasonic measurement covers a variety of models and types of flowmeters. The term “ultrasonic” does not unequivocally define the type of flowmeters. “Ultrasonic” merely indicates that the flow rate is measured using ultrasound. Actual flow is measured by either of three fundamentally different methods:
Transit time differential method (time-of-flight)
Doppler method
Cross-correlation method
The most applied and most accurate method is transit time differential (time of flight). It can be applied to liquid, gas, cryogenic (including LNG) and in high temperature applications.
Nowadays, a variety of ultrasonic sensor types are available for direct installation on the pipe or delivered preinstalled in a measuring tube. The sensors can be divided into three subgroups:
Clamp-on sensors
Insertion sensors
Inline sensors
Clamp-on sensors
Sound waves can pass through materials without causing damage. Medical diagnosis, materials testing, and flow measurement all make extremely good uses of this property. As far as measuring flow is concerned, this means that the sensor can be outside of the pipe and does not necessarily have to be in contact with the fluid. Devices mounted in this way are normally referred to as “clamp-on” sensors (Fig. 1). A characteristic of clamp-on sensors is that ultrasonic waves always pass through the centre of the pipe.
Fig. 1: Clamp-on sensors are mounted directly on the outside of a pipe. A special mounting rail facilitates exact positioning. Photo: Prosonic Flow clamp-on sensors from Endress+Hauser.
Sensors that are in direct contact with the fluid are known as “insertion or wetted sensors”. They are also used with multipath transit time meters, which have sound paths offset from the mid-plane of the pipe. Dual-path systems are an example (Fig. 3). Multipath systems offer a better linearity and are less susceptible to disturbance in the flow profile. Some manufacturers also offer insertion sensors that are hot tapped.
Fig. 2: Insertion sensors are fluid wetted. The sensor holder is welded into the pipe wall. Photo: Prosonic Flow insertion sensors from Endress+Hauser.
Measuring tube/in-line sensor
Prefabricated measuring tubes (see Fig. 3) are ideal for transposing laboratory-determined measuring accuracies directly to the site. An in-line sensor consists of a prefabricated measuring tube complete with preinstalled insertion sensors – which can be wetted or isolated from the fluid. Configurations like this generally employ in-line sensors with a multipath system consisting of two, three, four or more pairs of sensors.
Fig. 3: Prefabricated measuring tube with four insertion sensors and two measuring paths. Photo: In-line meter Proline Prosonic Flow G 300 from Endress+Hauser.
Frequently asked questions about ultrasonic flowmeters
We offer a complete portfolio for versatile and economical flow measurement of gases and liquids up to a nominal diameter DN 4000. Click here to see all ultrasonic flowmeters.
At the end of the course you will know about the features of the PROFINET technology and the PA profiles, network design of 100BaseTX and Ethernet-APL.
Would you like to participate at one of our events? Select by category or industry.
Respectăm confidenţialitatea dumneavoastră
Utilizăm module cookie pentru a optimiza experienţa dumneavoastră de navigare şi pentru a colecta date statistice în vederea optimizării funcţionalităţii site-ului web şi pentru a vă oferi reclame sau conţinuturi personalizate.
Prin selectarea opţiunii „Acceptare totală”, vă oferiţi consimţământul privind utilizarea modulelor cookie.
Pentru detalii suplimentare, vă rugăm să citiţi Politica noastră privind modulele cookie .